2021-09-22 06:32 AM
Hello, I read the Application note AN4602 about the start-up procedure of the LIS3MDL. When I change the mode of the sensor, the DRDY signal remains low and the sensor does not answer to the following I2C transactions.
Without changing the mode of the sensor, I am still able to read the measurement done during the start-up procedure and communicate with I2C with the sensor.
Does anyone had the same issue or has any suggestion?
Solved! Go to Solution.
2021-10-27 09:09 AM
I suspect an hardware issue on the PCB I am using. I plan to do some tests with a new sensor and PCB.
2021-09-24 07:29 AM
Hi @TGabo.2 ,
did you try to restart the measurment mode after changing modes?
as the AN says, The system goes to idle mode: • automatically at the end of startup procedure
this could be the problem
let me know if this solves it
Niccolò
2021-10-20 07:57 AM
Hi @TGabo.2 ,
do you have any update about your issue?
-Eleon
2021-10-27 09:09 AM
I suspect an hardware issue on the PCB I am using. I plan to do some tests with a new sensor and PCB.