2019-07-05 6:13 AM
Hi,
I interfaced LIS3DSH with Nordic controller(PCA10040). I am facing following issues:
please suggest any ways to solve this problems.
for your reference I am attaching data
Thanks & Regards,
Chaitanya.
2019-07-05 7:27 AM
Hi @chaitanya chippada , a few questions to understand the issue: are you correctly converting raw data into 16-bit two's complement data? Are you reading data in continuous mode and at which ODR? Vdd and VddIO have the same value? Regards
2019-07-07 10:22 PM
Hi Eleon,
Thanks for your reply,
are you correctly converting raw data into 16-bit two's complement data?
A. Yes, we are converting correctly, as some other data points is correct, following is the function we are using for converting raw value to g value.
int16_t two_compl_to_int16(uint16_t two_compl_value)
{
int16_t int16_value = 0;
/* conversion */
if (two_compl_value > 32768) {
int16_value = (int16_t)(-(((~two_compl_value) & (uint16_t)(0xFFFF)) + (uint16_t)(1)));
} else {
int16_value = (int16_t)(two_compl_value);
}
return int16_value;
}
Are you reading data in continuous mode and at which ODR?
A. we are reading data from sensor continously (stream mode)by giving required delay, for your reference I am attaching configured parameters, please suggest if any other settings required.
ret_code_t err = NRF_SUCCESS;
uint8_t reg[2] = {0x00};
reg[0] = MEMS_SENSOR_CTRL_REG4_ADDR;
reg[1] |= DATARATE_1600;
err = writeTolis3dsh(®[0], sizeof(reg));
APP_ERROR_CHECK(err);
reg[0] = MEMS_SENSOR_CTRL_REG4_ADDR;
reg[1] |= XYZ_ENABLE;
err = writeTolis3dsh(®[0], sizeof(reg));
APP_ERROR_CHECK(err);
reg[0] = MEMS_SENSOR_CTRL_REG3_ADDR;
reg[1] = 0x00;
err = writeTolis3dsh(®[0], sizeof(reg));
APP_ERROR_CHECK(err);
reg[0] = MEMS_SENSOR_CTRL_REG5_ADDR;
reg[1] |= FILTER_BW_800;
err = writeTolis3dsh(®[0], sizeof(reg));
APP_ERROR_CHECK(err);
reg[0] = MEMS_SENSOR_CTRL_REG5_ADDR;
reg[1] |= FULLSCALE_2;
err = writeTolis3dsh(®[0], sizeof(reg));
APP_ERROR_CHECK(err);
reg[0] = MEMS_SENSOR_CTRL_REG5_ADDR;
reg[1] |= (SELFTEST_NORMAL | SERIALINTERFACE_4WIRE);
err = writeTolis3dsh(®[0], sizeof(reg));
APP_ERROR_CHECK(err);
reg[0] = MEMS_SENSOR_CTRL_REG6_ADDR;
reg[1] |= (FIFO_ENABLE | AUTO_ADDRESS_INCREMENT);
err = writeTolis3dsh(®[0], sizeof(reg));
APP_ERROR_CHECK(err);
reg[0] = MEMS_SENSOR_FIFO_CTRL_ADDR;
//reg[1] |= FIFO_STREAM_MODE;
reg[1] = FIFO_STREAM_MODE;//0x40;//0x54;
err = writeTolis3dsh(®[0], sizeof(reg));
APP_ERROR_CHECK(err);
Vdd and VddIO have the same value?
A. Yes, Vdd & VddIO is same value 3.3 V
Thanks for your quick support,
Regards,
chaitanya
2019-07-09 2:37 AM
a few questions to understand the issue:
are you correctly converting raw data into 16-bit two's complement data?
A. Yes we are correctly converting raw data
Are you reading data in continuous mode and at which ODR?
A. We are reading in stream mode with 1.6KHz ODR
Vdd and VddIO have the same value?
VDD and Vddio have same value 3.3volts
Regards,
chaitanya
2019-07-24 7:14 AM
Do you have the same issue also at lower ODR? Regards