2013-12-19 08:28 AM
In LIS3DH datasheet (Doc ID 17530)
on figure 3 page 12/42 we can see: ''When no communication is on-going, data on CS, SPC, SDI and SDO are driven by internal pull-up resistors.'' What is the pull-up value? Are these pull-up still active if the LIS3DH is put in power down mode? #lis3dh-spi2017-02-22 07:47 AM
Still no support from STµ about the LIS3DH spi pull-up values?
Why is there a pull-up on SDA???? How can I guarantee that the last data bit from the microcontroller is a 1????
2017-02-23 01:29 AM
Please check the latest version of the datasheet for
http://www.st.com/resource/en/datasheet/lis3dh.pdf
.The datasheet says 'When no communication is ongoing, data on SDO is driven by internal pull-up resistors'.
So the pull-up is only on SDO/SA0 pin, the pull-up value can be found in chapter 1.1 and it can be disabled in CTRL_REG0.2017-06-14 10:48 AM
Is this pin still driven when the LIS3DH is in Power-Down mode (ODR=000 in CTRL_REG1)