cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2HH12TR Tap Detection Firmware Example

sean thakur
Associate
Posted on April 03, 2017 at 01:10

I have LIS2HH12TR on a PCB. I want to implement Tap Detection. I could not find a direct Register for configuring Interrupt for a tap. It would be great to refer to Example code for Tap Detection using Raw Accelerometer Data or any other alternative method using LIS2HH12TR?

#accelerometer #lis2hh12 #tap
2 REPLIES 2
Miroslav BATEK
ST Employee
Posted on April 04, 2017 at 18:01

Unfortunately LIS2HH12 doesn't have build in click/double-click recognition feature.

You would have to detect in by software.

RClab
Associate

The question: "... It would be great to refer to Example code for Tap Detection..."

This would be the software you are referring to.

Can someone provide example software, consisting of at least some device settings? Otherwise, one might conclude that it is difficult to implement.