2019-11-25 02:28 AM
Hello ST-Community!
When I'm using the LIS2DW12 at ODR=1.6kHz, the Interrupt for reaching the FIFO-Threshold is jittering with 1/ODR, but only if the threshold is greater than 12. If it's less or equal, everything is working fine.
The buffer-Mode is set to FIFO-Mode, but this behaviour also occurs in Continous-Mode.
The Power-Mode is set to High-Performance/Low-Noise.
The Interrupt is routed to the INT1-Pin
The two images show the rising edge on the pin INT1. The time between the two cursors "a" and "b" is 624us (almost 625us), which would equal to 1/ODR (1/1600 = 625E-6)
As written, this only happens if ODR is set to 1.6kHz and the FIFO-Threshold is greater than 12.
Does anyone have some further informations regarding this issue?
Thanks in advance for your answers!
Greetings,
Loris
2019-12-17 03:06 AM
Hi Eleon
The PCB was shipped today, so it will probably arrive by the end of the week.
If you have any questions, just let me know.
Regards,
Loris
2019-12-17 03:10 AM
Just at the beginning of the Christmas holidays ;) ok, let's see what we can do
Regards
2019-12-17 03:16 AM
Yeah, I know.
Timing at it's best... ;)
Thanks for your efforts!
2020-01-08 08:01 AM
Hi Loris, just received your board, thank you for your effort. I have some other question about the issue you are facing:
Regards
2020-01-10 12:09 AM
Hi Eleon
Regarding speeds:
The Sensor is running in FIFO-Mode (FMode[2:0] 001), so that doesn't solve the problem. But as far as I understand the Datasheet, in FIFO Mode the Sensor stops collecting Data as soon as there are 32 unread samples in the FIFO. But for me It's not really clear if this happens as well when the FIFO Threshold is reached (In my case 24).
I hope this helped you.
Regards,
Loris
2020-02-03 11:40 PM
Hi @Eleon BORLINI
Have you got any Updates for me?
Were you able to put the board in operation?
Thanks and Regards
Loris
2020-02-07 03:01 AM
Hi @Loris Wyss , unfortunately not yet, or, better, I'm still not able to reproduce the jitter failure...
Let me check again other configurations before coming back to you
Regards
2020-02-07 03:06 AM
Ok, thanks for the update.
Just for clarity: Can you see the described behaviour with the Hardware i sent you?
Regards
2020-02-28 04:56 AM
Hi @Eleon BORLINI
Have you found out anything regarding this Issue?
And have you been able to reproduce the described behaviour with the PCB i sent you?
Regards
2020-03-02 05:52 AM
Hi @Loris Wyss , I'm very sorry to come back to you without a news on your PCB... But I can ship back it to you, if you want. Btw, can you please check if your issue is somehow related to this other thread? Regards