2018-12-01 6:51 PM
I want to know how to do hardware or software reset on LIS2DE12TR when it does not work correctly.
2018-12-02 2:04 AM
There is not HW reset pin, the only solution to do HW reset is power cycle (Off/On).
You can reboot memory content by writing on to BOOT bit in CTRL_REG5 (24h), but this doesn't do full reset of the device.
On the other side there is not much reason why the device should work incorrectly.
2018-12-02 2:32 AM
I'm new to LIS2DE12TR. You mean, usually you don't have to think about the malfunction of LIS2DE12TR?
2018-12-02 9:08 AM
Yes.