2019-05-02 11:34 AM
Hello everyone,
I am conducting some tests with the STEVAL-BFA001V1B and STEVAL-IDP004V1 evaluation kit together with the STEVAL-IDP005V1 GUI software available on STSW-BFA001V1.
But I need to make some changes in the STEVAL-IDP005V1-GUI software, the source files for this softaware are made available and open for changes?
I am very grateful for any help or advice.
2019-05-08 03:31 AM
Hi, you can find the FW related to the STEVAL-IDP004V1 at this link. Which is your target application and which part of the firmware would you change? Regards
2019-05-08 05:37 AM
Hi Eleon,
The change I intend to make is in the "STEVAL-IDP005V1 GUI" software of the image below, I intend to include a graph with the average of the FFT of X, Y and Z, and also some other adjustments.
Does this software have open source code for testing and change?
I'm grateful for your attention.
2019-05-13 07:22 AM
Hi, I checked and unfortunately there seems to be no possibility to modify the GUI or get the source code, because it's a demo toolkit. I'll double-check and in case I'll come back to you. Regards
2019-05-13 08:52 AM
I understand Eleon, if you get the source code, I'll be very grateful.
Thank you for your great attention and understanding.
Best Regards