cancel
Showing results for 
Search instead for 
Did you mean: 

In FP-INT-PREDMNT, there is no IIS3DWB support for FFT Analysis?

Pasi MYLLYMAKI
ST Employee
 
1 REPLY 1
Vladimir JANOUSEK
ST Employee

In the FP-IND-PREDMNT1 the IIS3DWB can be of course also used and data source for the FFT calculation. There are also other accelerometers on the STWIN board , so user can recompile the project for his particular target setup / sensor configuration. In the BLE example shown during webinar ISM330DHCX is used due to limited BLE throughput.