2024-07-02 2:59 AM
Hi,
I am curretly using a Nucleo H503RB and the IKS02A1 expansion board in order to use the ISM330DHCX.
I tried several way to use via STM32Cube IDE which is my goal as i want to use C language without success to see any sign of an i2c adress with an i2c scan code.
When i used the Arduino ide with STM32Duino and the ISM330DHCX library it worked immediatly with the wire library i2c default instance.
What am i doing wrong in stm32cube ide ?
int main(void)
{
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ICACHE_Init();
MX_USART2_UART_Init();
MX_I2C2_Init();
MX_USART3_UART_Init();
MX_I2C1_Init();
/* USER CODE BEGIN 2 */
HAL_UART_Transmit(&huart3, StartMSG, sizeof(StartMSG), 10000);
uint8_t i = 0, ret;
for(i=1; i<128; i++)
{
ret = HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(i<<1), 3, 5);
if (ret != HAL_OK) /* No ACK Received At That Address */
{
HAL_UART_Transmit(&huart3, Space, sizeof(Space), 10000);
}
else if(ret == HAL_OK)
{
HAL_UART_Transmit(&huart3, StartMSG, sizeof(StartMSG), 10000);
}
}
HAL_UART_Transmit(&huart3, EndMSG, sizeof(EndMSG), 10000);
for(i=1; i<128; i++)
{
ret = HAL_I2C_IsDeviceReady(&hi2c2, (uint16_t)(i<<1), 3, 5);
if (ret != HAL_OK) /* No ACK Received At That Address */
{
HAL_UART_Transmit(&huart3, Space, sizeof(Space), 10000);
}
else if(ret == HAL_OK)
{
HAL_UART_Transmit(&huart3, StartMSG, sizeof(StartMSG), 10000);
}
}
HAL_UART_Transmit(&huart3, EndMSG, sizeof(EndMSG), 10000);
2024-07-02 3:04 AM
Please see the posting tips for how to properly post source code: