2017-04-26 12:12 PM
Hi, I am using
IIS328DQ in a new design. I want to set up an interrupt when the orientation is tilted away from Z-axis. So I set up INT1 as XHIE, XLIE, YHIE and YLIE. ZHIE and ZLIE are disabled.
Here is the setup sequence according an AppNote:
1. write CTRL_REG1
2. write CTRL_REG23. write CTRL_REG34. write CTRL_REG45. write Reference6. write INT1_THS7. write INT1_DUR8. write INT2_THS9. write INT2_DUR10. read HP_FILTER_RESET (if filter is enabled)11. write INT1_CFG12. write INT2_CFG13. write CTRL_REG5here is the reading of the sensor and all the registers:
AX -0.039
AY -0.063
AZ 0.965
WHO_AM_I : 0x32
CTRL_REG1 : 0x27
CTRL_REG2 : 0x08
CTRL_REG3 : 0xC0
CTRL_REG4 : 0x30
CTRL_REG5 : 0x00
HP_FLT_RST: 0x00
REFERENCE : 0x00
STATUS_REG: 0x00
OUT_X_L : 0x60
OUT_X_H : 0xFF
OUT_Y_L : 0x00
OUT_Y_H : 0xFF
OUT_Z_L : 0x70
OUT_Z_H : 0x0F
INT1_CFG : 0x0F
INT1_SRC : 0x6A
INT1_THS : 0x01
INT1_DUR : 0x32
INT2_CFG : 0x7F
INT2_SRC : 0x00
INT2_THS : 0x0F
INT2_DUR : 0x01
The problem is that, even though INT1_CFG=0x0F (ZHIE=0, ZLIE=0, YHIE=1, YLIE=1, XHIE=1, XLIE=1), the INT1_SRC shows 0x6A where ZH=1.
How can I solve this problem?
Thanks for help in advance.
-wwqiao
#iis328dq #interrupt2017-04-28 7:23 AM
The register INT1_CFG defines which condition will trigger the interrupt
Nevertheless the conditions are evaluated for all axis, so even if it is not selected in INT1_CFG you can see the result in INT1_SRC
To detect the orientation is tilted away from Z-axis you should set only XHIE and YHIE (INT1_CFG = 0x0A). If you enable both condition (higher, lower) it will be always true and the interrupt will be always triggered. Please be aware absolute value of acceleration in each axis is evaluated.
2017-05-05 12:33 PM
Hello Miroslav:
Thanks for reply and suggestion. But I am still confused a little.
We use the chip for an embedded system that sits in the mobile carrier in an industrial tool. We basically needs three functions:
(1) knowing exact orientations of the carrier.
(2) generating an interrupt when the carrier is tilted away from Z-axis.
(3) generating an interrupt when a shock happens.
The chip is configured as:
CTRL_REG1 : 0x27 (PM=001 (ODR Normal), DR=00 (50/37Hz), Zen=1, Yen=1, Xen=1)
CTRL_REG2 : 0x08 (BOOT=0, HPM=00 (normal), FDS=0 (HP Enabled), HPen2=1, HPen1=0, HPCF=00 (HPc=8))CTRL_REG3 : 0xE4 (IHL=1 (active low), PP_OD=1 (open drain), LIR2=1 (latch), I2_CFG=00 (I2 source), LIR1=1 (latch), I1_CFG=00 (I1 source))CTRL_REG4 : 0x80 (BDU=1 (block), BLE=0, FS=00 (00:2g, 01:4g, 11:8g), STsign=0, 0, ST=0, SIM=0)CTRL_REG5 : 0x00HP_FLT_RST: 0x00REFERENCE : 0x00(1) there is no difficulty to read and determine the orientations. However, I noticed it may report back the gravity over 1.0g (the chip is stationary). Do I need to normalize them by SQRT(X^2+Y^2+Z^2)?
(2) We try to use INT1 for the tilt detection. The requirement is small, 15 degree away from Z-axis. How do we understand the INT1_THS value? It is small if for Z-axis interrupt (ZHIE or ZLIE). It is big if for X- and/or Y-axis. Is the
INT1_THS value an absolute value? In other words, if we set it for XHIE and YHIE (your suggestion), what happens if X/Y reading value is minus? When the carrier is tilted away from Z-axis, X and/or Y reading could be positive or negative. How do we understand?
INT1 duration is set as 50 (at DR 50Hz, so about 1 second).
(3) for the shock detection, we set INT2_CFG : 0x7F (all 6 directions enabled and OR'ed). The threshold value sets 0.5g. INT2 has high-pass filter enabled. More or less, it generates interrupt. But we have observed that the INT2_SRC seems always indicate high event in XH, YH and ZH no matter what direction the chip sat and strikes applied. Can you shed lights?
INT2 duration is set as 1.
Thanks for helps in advance.
-wwqiao