2021-09-19 4:35 AM
I have spent some time on the forums and can see that there are many options for projects depending on the requirements of the user.
I am looking to hear people's opinions on a suitable setup as an introduction to the field. I am a firm believer in walking before you can run. My project is simple to record some vibration from a sensor and display it as an integer value.
No need for connectivity to std IoT protocols as yet.
I suppose one thing to consider is the availability of some products; eg, the STEVAL-STWINKT1B is out of stock now from many vendors available to me until after Xmas..
Another factor I am considering is, there are some setups that have great tutorials and examples I have seen one for the below mcu.
I was thinking of the STEVAL-MKI109V3 motherboard and STEVAL-MKI208V1K iNemo Inertial Module Kit?
Would be good to hear some opinions, the application is for motor, gearbox and pump condition monitoring via vibration.
Solved! Go to Solution.
2021-09-20 4:57 AM
In each project I create a doc file that shows how to create project from scratch.
History has shown that this takes relatively little time for the project writer to create, but a tremendous effort for the project inheritor.
If a similar project needs to be started, or the project somehow becomes corrupted, or the tools have been updated and the project didn't quite upgrade as expected, then this simple document is a life saver, and a huge time saver.
Paul
2021-09-20 4:57 AM
In each project I create a doc file that shows how to create project from scratch.
History has shown that this takes relatively little time for the project writer to create, but a tremendous effort for the project inheritor.
If a similar project needs to be started, or the project somehow becomes corrupted, or the tools have been updated and the project didn't quite upgrade as expected, then this simple document is a life saver, and a huge time saver.
Paul
2021-09-24 7:03 AM
Hi @thomas987adden ,
I can point you al so to STEVAL-MKSBOX1V1, that is similar to the STEVAL-STWINKT1B.
for any kit you want to try, the approach suggested by @Community member is a good one
Niccolò
2021-09-27 3:36 PM
An application of the IIS3DWB to vibration analysis posted here.