cancel
Showing results for 
Search instead for 
Did you mean: 

I am using Sensorile.BOX . I need a sample code or standard library , application notes and programming manual for Microphone TS922EIJT and MP23ABS1TR

Snara.21
Senior
 
12 REPLIES 12

Hi @Snara.2​ ,

please post this question on the STM32 group, topic STM32L4 (the one on the SensorTile.box): they'll be able to help you for sure more than me.

-Eleon

Hi @Snara.2​ ,

if you want to use the BLE communication, you have to use the "BLE" examples. The SDDataLogRToS example is for storing data in the SDD card.

0693W00000HpOA3QAN.png

-Eleon

Snara.21
Senior

@Eleon BORLINI​ 

Thanks for sharing the information. It works well. If I need to know the technical design parameters. How shall I find the infromations? For instance :- In SD Datalog RTOS - What is the RTOS Timer event configured, Crystal configuration, DFSDM Filter configuration with more details why this has been choosen and SD Card interface. Whether the MX file available.

If I need to create a new project and add the code what would be the detail procedure to integrate witt the existing project which I am working (Which has all sensors available in SEnsortile.Box + BT).