2021-12-17 9:04 PM
Hi,
we are trying to read FIFO buffer data but we are facing some issues in output data from FIFO
can anyone help me regarding the FIFO register setting
what is the value to be configured in the FIFO register?
2021-12-19 11:21 PM
Can any please reply for this
2021-12-20 3:58 AM
Hi @Sprem.1 ,
In absence of specific details about the issue, would first suggest you to read LSM6DSOX application note, FIFO modes, from p.101.
You can then have a loot to the Github examples in C, such as the lsm6dsox_fifo.c: these drivers implements the registers' settings, buffer reading and parsing in order to implement the FIFO mode on the LSM6DSOX.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-12-21 6:44 PM
Thank you so much eleon we will try this and let you know ASAP
2021-12-21 7:34 PM
Hi, eleon,
can we say whether this FIFO setting is correct?
FIFO_CTRL1(07h) - 0x00
FIFO_CTRL2(08h ) - 0x00
FIFO_CTRL3(09h) - 0xA0(gyroscope - 6667Hz)
FIFO_CTRL4(0Ah ) - 0x01(FIFO mode)
COUNTER_BDR_REG1(0Bh) - 0x00
COUNTER_BDR_REG2(0Ch) - 0x00
time sleep - 6ms (collecting 40 samples)
2021-12-22 1:35 AM
Hi @Sprem.1 ,
It should be OK, setting the FIFO mode this way. However, please pay attention to the gyro speed, which is quite high and which could cause the FIFO filling to fast without time to read it.
Otherwise, if you are facing issues, please try the online example (with your personal ODRs):
/*
* Set FIFO watermark (number of unread sensor data TAG + 6 bytes stored in FIFO) to 10 samples
*/
lsm6dsox_fifo_watermark_set(&dev_ctx, 10);
/* Set FIFO batch XL/Gyro ODR to 12.5Hz */
lsm6dsox_fifo_xl_batch_set(&dev_ctx, LSM6DSOX_XL_BATCHED_AT_12Hz5);
lsm6dsox_fifo_gy_batch_set(&dev_ctx, LSM6DSOX_GY_BATCHED_AT_12Hz5);
/* Set FIFO mode to Stream mode (aka Continuous Mode) */
lsm6dsox_fifo_mode_set(&dev_ctx, LSM6DSOX_STREAM_MODE);
/* Enable drdy 75 μs pulse: uncomment if interrupt must be pulsed */
//lsm6dsox_data_ready_mode_set(&dev_ctx, LSM6DSOX_DRDY_PULSED);
/* Set Output Data Rate */
lsm6dsox_xl_data_rate_set(&dev_ctx, LSM6DSOX_XL_ODR_12Hz5);
lsm6dsox_gy_data_rate_set(&dev_ctx, LSM6DSOX_GY_ODR_12Hz5);
-Eleon
2021-12-22 9:08 PM
Hi, eleon,
Thank you so much for your reply,
we are trying to run FIFO mode in a while loop but we observe that the FIFO buffer is not filling the second time
step 1: Configuration of Gyroscope control register and FIFO control register(6.6khz,2000dps,FIFO mode)
step 2: 100 ms delay --> 6.6Khz and 512 sample
step 3: while loop
step 4: reading x,y,z FIFO
step 5: Reading FIFO status register
step 6: 2s delay
step 7: Again Reading FIFO status register
step 8: Again it will go through step 3
can you suggest to me regarding this
2022-01-18 6:09 PM
Hi Team,
Finally, we got output from the FIFO buffer
ODR - 100 Hz(high-performance mode)
dps. - 2000 dps
FIFO mode - continuous mode
Sensor position - Rest position(static)
FIFO sample count :
Xdata : 8
Ydata : -4
Zdata : 0
Xdata : 8
Ydata : -6
Zdata : 1
Xdata : 7
Ydata : -5
Zdata : 4
But we are facing one issue in the 6.6 and 3.3KHz ODR sample count except for these two ODR all the ODR sample count is correct according to the datasheet while in the Rest position
ODR - 6.6KHz(high-performance mode)
dps. - 2000 dps
FIFO mode - continuous mode
Sensor position - Rest position(static)
FIFO sample count :
Xdata : -206
Ydata : -5
Zdata : 17
Xdata : 24
Ydata : 14
Zdata : 4
Xdata : 256
Ydata : 201
Zdata : -12
Can anyone suggest some point why in high ODR 6.66 and 3.33KHz it is behaving like this? If we want to operate the sensor in high ODR what to do can anyone please reply to this
2022-01-26 7:30 PM
Hi,
can anyone reply to the above query please
2022-01-27 7:00 AM
Hi @Sprem.1 ,
So you are reading higher acceleration values (from the FIFO) in the higher ODR case, right? Are you facing the same issue without passing though the FIFO?
I'm wondering if it could be effectively a measurement "issue", in the sense that in your setup there is a noise at high frequency (above the 1kHz ODR) that is detected only when you run the device at high ODRs.
You might also try to increase the SPI / I2C reading frequency: maybe the ODR is too high to be able to read the FIFO fast enough.
-Eleon