Does LSM6DSOX MLC have permanent memory?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-11-20 9:53 PM
1- Is there a permanent memory in LSM6DSOX for machine learning? In other words, does the ".ucf" file that we load in case of power off or reset become permanent?
2- Can we load the ".ucf" file without using "STEVAL-MKI109V3"?
3- Can we load the ".ucf" file using I2C communication?
Thank You.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-11-22 5:09 AM
Hi @bkrzn ,
The LSM6DSOX sensor has an embedded finite state machine (FSM) and machine learning core (MLC) which can be configured using a ".ucf" file. However, the sensor does not have non-volatile memory to store the ".ucf" file permanently. This means that if the sensor is powered off or reset, the configuration loaded from the ".ucf" file will be lost. You will need to reload the ".ucf" file each time the sensor is powered on or reset.
Yes, you can load the ".ucf" file without using the "STEVAL-MKI109V3". The "STEVAL-MKI109V3" is a convenient tool for evaluation and development, but it is not the only method to load the ".ucf" file. You can use any microcontroller or host processor that can communicate with the LSM6DSOX sensor via I2C or SPI interfaces to load the ".ucf" file.