2022-08-18 01:38 AM
Hello
We must replace the old LSM6DS with the new one LSM6DOX because of End of Life of the first one.
Checking the results on the same jig, reveals half of the Accelerometer part of the new chip.
Do you have a detailed documentation which may support with all the differences between them?
What should be change (in setup or in FW) in order to have the same results between them?
Thanks!
2022-08-18 01:42 AM
sorry for the misspelling - the old chip is LSM6DS3 and the new one is LSM6DSOX
2022-08-25 08:04 AM
2022-08-27 11:12 PM
HI
There are actually two problems:
I attached a PPT screen shot of the results comparison between the two: Please make the picture as bigger as you can to see the differences.
Thank you!
2022-09-14 06:25 AM
Hi @Evyatar Nassie ,
that's strange, are you configuring the two devices exactly in the same way (same ODR, FS, filters, etc...)? And did you test more than 1 device?
-Eleon