2019-08-26 06:08 PM
Hi,
I have setup the registers on the LIS3DSH according to the "Wake-up" example in application note AN3393. It works for the first interrupt, but so far i haven't had any luck to receive any more interrupts unless i read the OUTS1 register to reset it. I would like to keep on receiving interrupts without reading this register to save power not waking up the host MCU. Is there a way to do this?
Klas
2020-12-03 08:07 PM
Hi, Is your issue resolved? I have trouble writing into the registers according to the wake up example. and I had not luck getting any interrupt. can you guide me on the same?