2013-10-21 10:57 PM
I'm having trouble getting i2c communications working with LSM9DS0 iNEMO inertial module. I've wired it up, but it isn't responding to who_am_i read request. I've wired SDO to 1, so am using your default i2c address 0x3A, but I'm getting no slave ACK signals. Out of desperation wondering if I had the address wrong I pinged every i2c address, and still found no response. I've tried 100 kHz and 400 kHz, same result. I've also wired different i2c sensors, and they work fine, so I know the rest of my board works. Are there any tricks getting i2c to work?
2013-10-24 05:33 PM
bad soldering, got i2c working with gyro, still no luck with accelerometer...
2013-11-18 06:57 AM
Hello Chris,
I am currently verifying an answer for your topics. Please let me know if you have any advance or have any other questions. Thank you, Thiago Reis2014-06-04 02:42 AM
Me too have the same problem gyro is working but accelerometer is not working, is there any way to check whether it is a hardware problem or software problem or soldering problem
2015-01-21 01:27 PM
Hello,
I have same problem :( I haveLSM9DS0 and LPS25H on the same I2C bus, but only LPS25H responds. I don't believe it's a soldering problem because i have made two boards to specially rule out random component and soldering faults. Also i've inspected them under microscope.
Anybody have some idea?2015-02-03 01:40 PM
It still was a soldering problem on both boards... :S