2018-10-04 7:54 AM
Hi, I have an LIS2DW12 fitted to a STEVAL-MKI179V1 board. I have it connected to a microcontroller programmed to set an interrupt pin on wake up as per DT0098. The interrupt pin goes high with a light tap in the xy or z axis. However I want it to detect angular movement in any plane due to gravity. How do I achieve this? Is it to do with the HF filter? Any help appreciated. Thanks, Dave.
2018-10-04 9:42 AM
2018-10-04 10:15 AM
I'll have a look Miroslav. I want it to wake up with 1 degree of movement. Thanks, Dave
2018-10-05 2:18 AM
Not really what I'm looking for. At the moment using the pseudo code in ST Design Tip DT0098 I get an interrupt output whenever the device accelerates in any axis but it seems to ignore the gravity element.
Tilting the device will not set the interrupt. Am I missing something? Thanks, Dave.
2018-10-25 12:07 AM
I don't know which pseudo code (configuration) you use because there is several examples in the DT0098.
What would be starting position? Do you really need to detect angular movement of 1 degree?
If you want to wake up some device when it moves you don't have to detect exactly one degree tilt.
If you would explain exactly what you want to achieve I can probably advise you souitable sensor configuration.
2020-10-07 1:33 PM
@Miroslav BATEK .
Hi ,
I have found this tag while searching about a solution for tilt angle measurement. I uses LIS2DW12. I have seen that 6D orientation angle is from 45-50 degrees only.
I would like to wake up on minimum angle flexible tilt say 5degree/10 degree . How could I achieve It. Is there any pseudo code for that?. When checked the STmem driver, I have seen that WAKE_UP_THS(34h) for setting threshold values. How I can get interrupt for a tilt value(say 10 degree) for only one axis by setting threshold in this register.
regards,
SV