2019-09-02 12:01 AM
2019-09-24 3:51 AM
2019-09-24 2:52 PM
Thank you for your reply. Right now, I am applying the kalman filter algorithm to remove the drift,this is the process I must do in my project, there is a matrix R,which is the variance of the measurement. I read the paper says it should provided by the company. Do you have idea what that is?
And another thing surprise me is, why your device even have no drift?After I run the device about 5 mins, the gyroscope is still very accurate? Does this device already have some inner functions to remove drift?
2019-09-25 6:10 AM
Hi @Sunny.Q , I was wrong suggesting you the use of MotionEC compass library, which of course uses the axl+mag data. The right FW package is MotionFX one, in 6-axis mode. However, it's not directly possible to get the Matrix Q from that source code, too deep inside the algorithm. Sorry for the lack of help :crying_face: Regards