cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, Can you please suggest STM MCU/MPU part which is used for 3 phase metering applications?

BKath
Associate II

We are looking for the MCU parts which should have below features.

  1. 512Kb flash, 64Kb RAM
  2. 12 Bit 12-16 channels Delta Sigma ADCs
  3. SPI,I2C, UART, CAN, USB2.0
  4. LCD Interface
  5. External RAM interface up to 512Mb
  6. External Flash interface up to 64Mb
  7. 80 -100 GPIOs
  8. DAC
  9. SD/MMC Interface

Thanks,

Brijesh K.

1 REPLY 1