cancel
Showing results for 
Search instead for 
Did you mean: 

H3LISD331DL Accelerometer Accuracy

bjackson96
Associate II

Hello,

I have been working on a project using the H3LISD331Dl accelerometer set at +-400g and the STM32U585OI MCU. I wish to capture the high G shocks that occur during drop testing. I have completed my project and I am just wondering how accurate the results I am getting are. I secured my PCB inside an enclosure and did drops from various different heights focused on different axis. I attached .csv files for 3ft and 6ft drops focused onto the Z-axis. I plotted the data I got in excel and the increase in g's seem to correlate with the increase in drop height. Is there any way to guarantee the accuracy of the values I am recording? 

0 REPLIES 0