2024-07-22 07:19 AM
Hello,
The LIS2DUX12 datasheet clearly states that "12.1.3 FSM_START_ADD_L (58h) and FSM_START_ADD_H (59h) FSM start address register (R/W). First available address is 0x35C.".
The default address in MEMS-studio is 0x0200. In the FSM examples on GitHub, the address also is the same: 0x0200.
Why are these addresses different and which one is correct?
Solved! Go to Solution.
2024-09-04 05:29 AM
Hi @zmogas ,
Thank you for reporting us the misalignment in FSM Start address definition between examples and datasheet.
We will update the datasheet in order to expose 0x19C as first available address for FSM. (We will keep 0x0200 in our examples/applications since it is of course a valid start address)
2024-09-04 05:29 AM
Hi @zmogas ,
Thank you for reporting us the misalignment in FSM Start address definition between examples and datasheet.
We will update the datasheet in order to expose 0x19C as first available address for FSM. (We will keep 0x0200 in our examples/applications since it is of course a valid start address)