cancel
Showing results for 
Search instead for 
Did you mean: 

FSM_START_ADDRESS in LIS2DUX12

zmogas
Associate II

Hello,

The LIS2DUX12 datasheet clearly states that "12.1.3 FSM_START_ADD_L (58h) and FSM_START_ADD_H (59h) FSM start address register (R/W). First available address is 0x35C.".

The default address in MEMS-studio is 0x0200. In the FSM examples on GitHub, the address also is the same: 0x0200.

Why are these addresses different and which one is correct?

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @zmogas ,

Thank you for reporting us  the misalignment in FSM Start address definition between examples and datasheet.

We will update the datasheet in order to expose  0x19C as first available address for FSM. (We will keep 0x0200  in our examples/applications since it is of course a valid start address)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @zmogas ,

Thank you for reporting us  the misalignment in FSM Start address definition between examples and datasheet.

We will update the datasheet in order to expose  0x19C as first available address for FSM. (We will keep 0x0200  in our examples/applications since it is of course a valid start address)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.