cancel
Showing results for 
Search instead for 
Did you mean: 

Flashing STEVAL-MKSBOX1V1 with STLINK-V3 not working?

TVan .2
Associate II
 
13 REPLIES 13

Thanks, Eleon.

I already have the ST LINK V2 adapter kit with cables and also the parts ability to make additional cables, if needed. My connections via STM32CubeProgrammer (Debian Linux and Oracle JRE8) and STLINK V2 appear to be working as they should.

TJM

Hello Eleon,

The adapter's been arrived, thank you,

the SensorTile.Box talks with V2, but not with V3 + B-STLINK-VOLT

Best regards

>> but not with V3 + B-STLINK-VOLT

I'm waiting for internal feedback... I'll let you know asap. Regards

Hello Eleon,

I made some further tests, after the configuration sucessfuly tested yesterday doesn't want to work on another desk today,

the problem lays on some kind of interferences,

the V2 is clocked just with 4MHz, the V3 with 24MHz

so the default 4 MHz of V2 usually allows the connection with Tile.Box, however not always

setting it down to 1,8MHz or 0,95MHz makes it more stable

so going further that way, I found that even V3 (with voltage converter) is able to connect, but with a clock not faster than 0,2MHz, which is very slow in fact

BR