2020-03-07 8:44 AM
2020-07-14 8:11 AM
Thanks, Eleon.
I already have the ST LINK V2 adapter kit with cables and also the parts ability to make additional cables, if needed. My connections via STM32CubeProgrammer (Debian Linux and Oracle JRE8) and STLINK V2 appear to be working as they should.
TJM
2020-07-16 5:27 AM
Hello Eleon,
The adapter's been arrived, thank you,
the SensorTile.Box talks with V2, but not with V3 + B-STLINK-VOLT
Best regards
2020-07-16 5:40 AM
>> but not with V3 + B-STLINK-VOLT
I'm waiting for internal feedback... I'll let you know asap. Regards
2020-07-17 6:08 AM
Hello Eleon,
I made some further tests, after the configuration sucessfuly tested yesterday doesn't want to work on another desk today,
the problem lays on some kind of interferences,
the V2 is clocked just with 4MHz, the V3 with 24MHz
so the default 4 MHz of V2 usually allows the connection with Tile.Box, however not always
setting it down to 1,8MHz or 0,95MHz makes it more stable
so going further that way, I found that even V3 (with voltage converter) is able to connect, but with a clock not faster than 0,2MHz, which is very slow in fact
BR