cancel
Showing results for 
Search instead for 
Did you mean: 

consume very high current in lsm6dsox

Sprem.1
Associate III

Hi team,

we have configured accelerometer normal mode in the sensor

Below configuration - Accelerometer normal mode

Power mode - Normal mode

G-Range - 16 g

ODR

  • 208HZ

CTRL8_XL (0x00)

CTRL6_C (0x10)

CTRL1_XL (0x54)

  • 104 HZ

CTRL8_XL (0x00)

CTRL6_C (0x10)

CTRL1_XL (0x44)

From this, we observe that the duty cycle is correct but the current is very high.

we are using the host as CC2652RB and slave as lsm6dsox using spi communication

can anyone help us with this

0693W00000F9wNBQAZ.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
Sprem.1
Associate III

Hi Niccolo,

Finally, we found the solution to this. we followed the lsm6dsox application note for the register setting.

View solution in original post

3 REPLIES 3
Sprem.1
Associate III

Can any one ​please reply for this

niccolò
ST Employee

Hi @Sprem.1​ ,

are the connections on the schematic like the ones shown in the datasheet on page 39 (figure 24)?

are SDx and SCx connected to GND or to VDDIO?

Niccolò

Sprem.1
Associate III

Hi Niccolo,

Finally, we found the solution to this. we followed the lsm6dsox application note for the register setting.