cancel
Showing results for 
Search instead for 
Did you mean: 

Can't manage to use multiple blocks of the same type on MEMS Studio

aesteban
Associate III

Hi, I noticed that, on MEMS Studio, whenever a block is repeated inside a subdesign it gives an error when building. As an example to represent this, I've created a subdesign "A" where I input the acceleration sensor of a X-NUCLEO IKS01A3 and i output the results in a graph as shown in the next image.

aesteban_0-1718697699993.png

The subdesign "A" uses a demux, adds to every output its current value with the previous one and mux it back again.

aesteban_1-1718697880426.png

The given error references to undeclared variables of the repeated blocks as shown below:

aesteban_2-1718698045973.png

Any advice on how to prevent this from happening?

Thanks in advance

 

1 ACCEPTED SOLUTION

Accepted Solutions
Miroslav BATEK
ST Employee

Hello @aesteban,

thank you for highlighting this bug. It is fixed in the new release of MEMS Studio v1.3.0. 

View solution in original post

1 REPLY 1
Miroslav BATEK
ST Employee

Hello @aesteban,

thank you for highlighting this bug. It is fixed in the new release of MEMS Studio v1.3.0.