2019-06-06 1:29 PM
Hi,
I'm facing with a issue on unicleo gui and sensorTile sensor (with ALLMEMS1 and ALLMEMS2 librairies).
I dont know why, but since few day i can pair and connect my sensor tile with bluetooth on my laptop (W10) but unicleo doesn't show the normal interface with sensor picture and librairies selection.
i try to update my bluetooth driver, update gui to 1.8, uninstal/install all driver and soft but same pb!
Is anybody encountered the same pb, and have a workaround?
For finish, sensorTile work fine with Android STBLE app!
thanks
2019-06-06 11:57 PM
Hi,
unfortunately the ALLMEMS2 FW is not yet supported.
Could you please try again ALLMEMS1 and if it doesn't work send us a screenshot.
I double checked it now with Unicleo-GUI 1.8.0 and ALLMEMS1 3.4.0 and it works fine for me.
2019-06-07 1:13 AM
Hi,
Many thanks for your answer!
So I try with the same setting ALLMEMSV340 and unicleo 1.8, and it work fine!
Do you know if ALLMEMSV2 will soon be supported or not?
Thanks
2019-06-07 2:29 AM
We will try to add it in the next release in a few weeks.
2020-05-27 4:55 AM
I have a similar issue. I have just acquired a SensorTile.box (STEVAL-MKSBOX1V1) board and I fail to connect to Unicleo-GUI (runs on Win10). While I am able to pair the device to my Win10 Machine (I can find it in the Paired Bluetooth devices on Win10), the Unicleo-GUI doesn't seem to see it.
I was able to connect it to my phone and managed to read data from it, but need to switch to the PC. please help
2020-05-27 6:12 AM
Did you enable the BLE support in Unicleo-GUI settings?
2020-05-27 6:13 AM
sure I did. and also restarted the app as instructed (even rebooted the machine).
I have tried this on 2 different Win 10 Machines, same thing happened
2020-05-27 6:19 AM
Can you make a screenshot of the list of paired Bluetooth devices in Windows and screenshot of the Select Device combo box in Unicleo-GUI?
What is the FW in your SensorTile.box?
2020-05-27 6:27 AM
2020-05-27 6:27 AM