2023-01-22 11:10 AM
I am using Nucleo F767ZI with SPI interface to ASM330LHHX sensor.
I am using example code from https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/asm330lhhx_STdC/examples/asm330lhhx_read_data_polling.c
After a couple of seconds "asm330lhhx_xl_flag_data_ready_get" allways returns 0.
After power off and power on I get a couple of readings but then again nothing.
What am I doing wrong?
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_SPI4_Init();
/* USER CODE BEGIN 2 */
platform_init();
platform_delay(BOOT_TIME);
do{
asm330lhhx_device_id_get(&dev_ctx, &whoamI);
HAL_Delay(1);
}while(whoamI != ASM330LHHX_ID);
/* Restore default configuration */
asm330lhhx_reset_set(&dev_ctx, PROPERTY_ENABLE);
do {
asm330lhhx_reset_get(&dev_ctx, &rst);
} while (rst);
/* Disable I3C interface */
asm330lhhx_i3c_disable_set(&dev_ctx, ASM330LHHX_I3C_DISABLE);
asm330lhhx_i2c_interface_set(&dev_ctx, ASM330LHHX_I2C_DISABLE);
/* Enable Block Data Update */
asm330lhhx_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/* Set Output Data Rate */
asm330lhhx_xl_data_rate_set(&dev_ctx, ASM330LHHX_XL_ODR_833Hz);
asm330lhhx_gy_data_rate_set(&dev_ctx, ASM330LHHX_GY_ODR_833Hz);
/* Set full scale */
asm330lhhx_xl_full_scale_set(&dev_ctx, ASM330LHHX_2g);
asm330lhhx_gy_full_scale_set(&dev_ctx, ASM330LHHX_2000dps);
asm330lhhx_xl_hp_path_on_out_set(&dev_ctx, ASM330LHHX_LP_ODR_DIV_100);
asm330lhhx_xl_filter_lp2_set(&dev_ctx, PROPERTY_ENABLE);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
uint8_t reg;
/* Read output only if new xl value is available */
asm330lhhx_xl_flag_data_ready_get(&dev_ctx, ®);
if (reg)
{
/* Read acceleration field data */
memset(data_raw_acceleration, 0x00, 3 * sizeof(int16_t));
asm330lhhx_acceleration_raw_get(&dev_ctx, data_raw_acceleration);
acceleration_mg[0] = asm330lhhx_from_fs2g_to_mg(data_raw_acceleration[0]);
acceleration_mg[1] = asm330lhhx_from_fs2g_to_mg(data_raw_acceleration[1]);
acceleration_mg[2] = asm330lhhx_from_fs2g_to_mg(data_raw_acceleration[2]);
HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
}
asm330lhhx_gy_flag_data_ready_get(&dev_ctx, ®);
if (reg)
{
/* Read angular rate field data */
memset(data_raw_angular_rate, 0x00, 3 * sizeof(int16_t));
asm330lhhx_angular_rate_raw_get(&dev_ctx, data_raw_angular_rate);
angular_rate_mdps[0] =asm330lhhx_from_fs2000dps_to_mdps(data_raw_angular_rate[0]);
angular_rate_mdps[1] =
asm330lhhx_from_fs2000dps_to_mdps(data_raw_angular_rate[1]);
angular_rate_mdps[2] =
asm330lhhx_from_fs2000dps_to_mdps(data_raw_angular_rate[2]);
HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
}
asm330lhhx_temp_flag_data_ready_get(&dev_ctx, ®);
if (reg)
{
/* Read temperature data */
memset(&data_raw_temperature, 0x00, sizeof(int16_t));
asm330lhhx_temperature_raw_get(&dev_ctx, &data_raw_temperature);
temperature_degC = asm330lhhx_from_lsb_to_celsius(data_raw_temperature);
}
HAL_GPIO_TogglePin(LD1_GPIO_Port, LD1_Pin);
HAL_Delay(100);
}
2023-04-12 2:58 AM
Hi @MAnto.2 ,
Are you confident about the stability of Vdd and Vddio?
2024-03-21 11:41 AM
Hi,
I have the same problem. Do you find a solution ?
Thanks in advance for your help...