2017-08-30 06:21 AM
I am wondering why the LSM6DSL does not have a design tip for calibration like the LSM6DS3 (DT0053, DT0059)
are these documents not valid for the LSM6DSL ?
2017-08-31 05:10 AM
The mentioned design tips are generic and can be used also for LSM6DSL.
I can also recommend you to have a loot at
package which contains libraries for accelerometer, gyroscope and magnetometer calibration.