2018-05-22 11:18 PM
Hello, I'm going to develop a kind of solutions for local positioning, and wondering the benefits of using integrated sensors (accelerometer, gyro, and magnetometer) like LSM9DS1 over using individual sensors and gathering.
As I can handle each sensor like LSM6DSL and LIS2MDL, I think I can make data like from LSM9DS1.
Are the data from LSM9DS1 sensor better in terms of accuracy, speed, or any other things?
Thank you for your answer in advance!
#mems #lsm9ds1Solved! Go to Solution.
2018-05-23 07:37 AM
The only benefit which I see is that all is in one package, so the occupied area on PCB is smaller.
But the LSM9DS1 is quite old device, the combination of LSM6DSL + LIS2MDL is much better option.
In terms of accuracy, current consumption, embedded features, and so on the combination of these two devices is much better.
2018-05-23 07:37 AM
The only benefit which I see is that all is in one package, so the occupied area on PCB is smaller.
But the LSM9DS1 is quite old device, the combination of LSM6DSL + LIS2MDL is much better option.
In terms of accuracy, current consumption, embedded features, and so on the combination of these two devices is much better.