2020-09-16 08:09 PM
Hi, recently I got a X-NUCLEO-BNRG2A1 and I am trying to use it with NUCLEO-G070RB without success. I have created a project with STM32CubeMx assistance using SampleApp of X-CUBE-BLE2, mapping the pins of the expansion board to my nucleo board as follows:
RST - PA8
SPI_SCK - PA5
SPI_MOSI - PA7
SPI_MISO - PA6
CS - PA1
SPI_EXTI_IRQ - PA0
The project successfully built and uploaded into the MCU, however the application does not do anything it just stuck in the function HCI_TL_SPI_Reset. I have already tried installing the DTM hex file into X-NUCLEO-BNRG2A1, however it does not solve the problem.
is it a problem of the DTM software?
2020-09-23 11:39 AM
I manage to make it work! However I am not sure why using the STM32CubeMx does not work. The problem appears to be the SPI frequency (it must be 1MHz). It works with a HAL that I developed, but it does not work with ST HAL, I don't know if I am doing something wrong.
2020-09-23 12:45 PM
Congrats! Look out at the PREESCALER which determines the final baudrate.
I also make mine work!
At the *ioc->Software Pack -> Select Component -> X-CUBE-BLE2 if configured HCI_TL as "Basic" and HCI_TL_INTERFACE as "Template".
Using the "Template" I still need to configure some functions to send/receive SPI.
I was trying to make it works using the "User board" option in the HCI_TL_INTERFACE... and that didn't work because it reconfigured lots of pins and the spi port itself... the CubeMX generator was a mess with this example.
Thanks for your support :D
2020-09-23 12:58 PM
Thank you too, I had given up, but when I saw that there was someone else with this problem, I tried again.
I manage to get it work with UserBoard too, STCubeMx does not put the interrupt handler, so that's why it got stuck there, I just add this to the stm32g0xx_it.c (in my case):
void EXTI0_1_IRQHandler(void)
{
HAL_EXTI_IRQHandler(&H_EXTI_0);
}
And that's it.
Thanks for your support, too.
2022-12-20 10:11 PM
hi @PFuen.1 did you resolved the issue? if yes can you help me out with the same. I too not able to even initiate the bnrg2a1, its getting stuck in one of the while loop after getting gatt init failed, bdarr failed.
2022-12-20 10:38 PM
@satyam9896 hi, yes I did, however I don't remember exactly what it was.
- You should check if "hci_tl_lowlevel_isr" is called in the external pin interrupt.
- SPI MUST have this configuration:
ClockPhase: LL_SPI_PHASE_2EDGE
ClockPolarity: LL_SPI_POLARITY_LOW
Note that LL_SPI_PHASE_2EDGE and LL_SPI_POLARITY_LOW belongs to the LL driver, but you can find the equivalent for the HAL library easily as they should have a similar name.
2022-12-21 03:42 AM
I'm attaching the ss for simpler changes which you said . i just wanted to know regarding hci_tl_lowlevel_isr that it is correct ay to call ?
2022-12-21 03:45 AM
2022-12-21 04:06 AM
still im getting same errors.
2022-12-21 08:05 AM
@satyam9896 Hmm no, remove "hci_tl_lowlevel_isr" from there. When using the HAL it should be done with the function HAL_EXTI_RegisterCallback. You have to only check that you have this in "stm32xxx_it.c":
void EXTI0_IRQHandler(void)
{
HAL_EXTI_IRQHandler(&H_EXTI_0);
}
And that in "hci_tl_interface.c", the function hci_tl_lowlevel_init has attached "hci_tl_lowlevel_isr" into the interrupt:
void hci_tl_lowlevel_init(void)
{
tHciIO fops;
/* Register IO bus services */
fops.Init = HCI_TL_SPI_Init;
fops.DeInit = HCI_TL_SPI_DeInit;
fops.Send = HCI_TL_SPI_Send;
fops.Receive = HCI_TL_SPI_Receive;
fops.Reset = HCI_TL_SPI_Reset;
fops.GetTick = BSP_GetTick;
hci_register_io_bus (&fops);
HAL_EXTI_GetHandle(&hexti0, EXTI_LINE_0);
HAL_EXTI_RegisterCallback(&hexti0, HAL_EXTI_COMMON_CB_ID, hci_tl_lowlevel_isr); // <--- THIS
HAL_NVIC_SetPriority(EXTI0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI0_IRQn);
}
Also, make sure that whenever "MX_SPIx_Init" is defined, it must have this configuration:
hspi->Init.CLKPolarity = SPI_POLARITY_LOW;
hspi->Init.CLKPhase = SPI_PHASE_2EDGE;
2022-12-21 10:06 PM
hi, i have done all three changes done but still its showing same errors.