cancel
Showing results for 
Search instead for 
Did you mean: 

Which WiFi module is best fit to use with STM32F103C8T6 controller?

vishweshgm
Associate II

I want a project to be done urgently using STM32F103C8T6 controller using CUBEMX. This project has a requirement of sending some measured data to cell phone using mobile's hotspot (and not using internet. Basically I need to send it through TCP/IP). I tried using ESP8266 but couldnot find the proper libraray implementation for the same that I can use easily. Can you guys recommend a best wifi module that I can use with this controller and get the project ready soon. Appreciate the library links in the answer description. Cost of the module does not matter.

1 REPLY 1
Aydn22
Associate

Which one did you use