cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX ILI9341 parallel 8-bit - Black Screen

JPolj.1
Associate

I'm trying to set up TouchGFX on an ILI9341 screen. Board is NUCLEO-L476RG. The screen is connected in parallel in 8-bit mode

For example if I draw a white box over the entire screen in TouchGFX designer, ILI9341 displays a white screen, If I draw a black box over the entire screen in TouchGFX designer, ILI9341 displays a black screen, But if i draw button or some similar, ILI9341 showing only black screen. I'm not sure if my code is wrong (I'm a beginner) or if TouchGFX has a some bug.

TouchGFXDataTransfer.c

#include "ili.h"
#include "TouchGFX_DataTransfer.h"
 
extern void DisplayDriver_TransferCompleteCallback();
 
static uint8_t isTransmittingData = 0;
 
uint32_t touchgfxDisplayDriverTransmitActive(void)
{
	return isTransmittingData;
}
void touchgfxDisplayDriverTransmitBlock(uint8_t* pixels, uint16_t x, uint16_t y, uint16_t w, uint16_t h)
{
	isTransmittingData = 1;
	ILI9341_SetWindow(x, y, x+w-1, y+h-1);
	ILI9341_DrawBitmap(w, h, pixels);
	isTransmittingData = 0;
	DisplayDriver_TransferCompleteCallback();
}

ILI9341.c

void ILI9341_DrawBitmap(uint16_t w, uint16_t h, uint8_t *s)
{
	for(uint16_t broj=0;broj<w*h*2;broj++)
	{
		LCD_WR_DATA(*(s));
 
	}
}

main.c

/* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART2_UART_Init();
  MX_SPI3_Init();
  MX_SPI2_Init();
  MX_CRC_Init();
  MX_TIM2_Init();
  MX_TouchGFX_Init();
  /* USER CODE BEGIN 2 */
  HAL_TIM_Base_Start_IT(&htim2);
  ILI9341_Init();
 
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
 
    /* USER CODE END WHILE */
 
  MX_TouchGFX_Process();
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}
 
 
/* USER CODE BEGIN 4 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
	extern void touchgfxSignalVSync(void);
		if (htim->Instance == TIM2) {
		touchgfxSignalVSync();
	}
}
 
/* USER CODE END 4 */

The hardware and the ILI9341 library are fine because I successfully launched LVGL on the same configuration.

2 REPLIES 2
MM..1
Chief III
JPolj.1
Associate

I solved the problem. Everything is fine now. I made a mistake in the function to transfer the framebuffer to the screen.

I wrote

LCD_WR_DATA(*(s));

I forgot to add a variable to increment the framebuffer pointer.

LCD_WR_DATA(*(s+number));

Thanks for your help..