2023-11-17 1:15 AM
Hello Team,
We have one project where we customer used the ST3485EIDT IC for RS485 communication.
By looking the schematic design we see that DI pin is connected with UART Tx pin but its series resistor has been removed.
We checked the functaonlity and found that device is able to do the Transmit and Receive.
We are unable to understand logic by exploring the datasheet.
Kindly do the helpfull if something needs to impliment in the design or not.
Solved! Go to Solution.
2023-11-17 4:35 AM
Welcome @pratikpanchal44, to the community!
In your schematics, R133 is not populated (DNP = Do Not Populate), so DI is connected to GND via R123 (0 ohms). However, transmission during communication only takes place via the line drivers for input signal 1, and via the pull resistors R93 and R94 for input signal 0:
Summary: the communication will work for short distances. However, you should experience increasing problems as the distance increases because the pull resistors cannot completely replace the impedance of the line drivers. Figuratively speaking, you turn on the tap to push water into the pipe when sending a 1. However, when the tap is switched for reverse direction, the water is no longer sucked back, but slowly drips past the tap.
I would recommend to take another close look at the circuit in the overall concept of your system (distance to be bridged, data rate, data to be transmitted, etc) and thoroughly rethink the control of the ST3485 on /RE, DE and DI.
Hope that helps?
Regards
/Peter
2023-11-17 4:35 AM
Welcome @pratikpanchal44, to the community!
In your schematics, R133 is not populated (DNP = Do Not Populate), so DI is connected to GND via R123 (0 ohms). However, transmission during communication only takes place via the line drivers for input signal 1, and via the pull resistors R93 and R94 for input signal 0:
Summary: the communication will work for short distances. However, you should experience increasing problems as the distance increases because the pull resistors cannot completely replace the impedance of the line drivers. Figuratively speaking, you turn on the tap to push water into the pipe when sending a 1. However, when the tap is switched for reverse direction, the water is no longer sucked back, but slowly drips past the tap.
I would recommend to take another close look at the circuit in the overall concept of your system (distance to be bridged, data rate, data to be transmitted, etc) and thoroughly rethink the control of the ST3485 on /RE, DE and DI.
Hope that helps?
Regards
/Peter