cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01SA SPWF01SC Data Rate?

Posted on October 03, 2014 at 00:49

Hi

What's the max bps/symbol-rate for SPWF01SA/SPWF01SC?

thx

#data-rate #symbol-rate #bps
13 REPLIES 13
Posted on February 01, 2017 at 11:43

How does this answer relate to this: 

https://community.st.com/0D50X00009XkeHySAJ

 

Which is correct 40-50kB/s or 1Mbps (which is approx 100kB/s)?
Posted on February 01, 2017 at 18:22

1MB is baudrate, 50KB is 'goodput' (amount of bits moved over the air in 1 seconds)

Posted on February 02, 2017 at 08:46

Ok. I tested 480600 baud/sec and that had around 40kB of data througput using http connections (I could not reach the same data rate using sockets, though).

So I assume that the 50kB/s limit is due to the firmware implementation. Do ST provide a firmware for 

SPWF01SA with SPI exposed for higher throughput? Or is it possible to change the firmware ourselves? 

Posted on February 02, 2017 at 11:10

Please contact your local ST office, or distributor...