cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01: Module enters IP 192.168.0.50

florian239955_st
Associate II
Posted on January 30, 2017 at 16:55

Hi,

my modules are sometimes returning the IP address 192.168.0.50 since they already had another IP address from the access point. When they got the IP address 192.168.0.50, I can't connect to them via TCP anymore. Then I have to reset the device.

Does anyone has this behavior, too? Or has an idea why the modules change it's IP address?

Regards,

Flow

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Gerardo GALLUCCI
ST Employee
Posted on February 01, 2017 at 19:00

Hi Flow,

that IP address is the one used when module's DHCP client is turned off. Variable ip_use_dhcp set to 0.

If you have a DHCP server on your network (and variable is set to 1), it is releasing a good IP to module.

I don't expect that address when DHCP server/clien are running.

florian239955_st
Associate II
Posted on February 02, 2017 at 08:33

Hi Jerry,

I know that this is the default IP address. The strange thing is, that the device already had another IP address given by the access point. Sometimes it switches than to 192.168.0.50. Debugging will go on...

Best regards,

Flow