cancel
Showing results for 
Search instead for 
Did you mean: 

SPBTLE-1S not working?

astrone
Associate

0690X000008BZnYQAW.png0690X000008BZnJQAW.pngHey everyone.

i have connected the following pins from the SPBTLE-1S to the ST Link V2.

SPBTLE-1S | ST LInk V2 JTAG connector

Vin (pin 5) | VDD (pin 19) & VAPP (pin 1 & 2)

GND (pin 8) | GND (pin 16 & 18)

SWCLK (pin 12) | SWCLK (pin 9)

SWDIO (pin (13) | SWDIO (pin 7)

RST (pin 19) | NRST (pin 15)

I have attached pictures of the pin descriptions from both modules.

can anyone tell me why i dont get any connection/communication to the BLE-module?

i get the error message as shown in the picture below. And i use the settings that is shown in the picture.

0690X000008BZp0QAG.png

Any suggestions ?

0 REPLIES 0