cancel
Showing results for 
Search instead for 
Did you mean: 

While sending the data from the app to node which function call calls first to receive the sent data?

Anitha
Associate III

I'm sending some data from nRF Connect app to node I want too see that data in firmware debugging. Where can I see that data? I mean in which function call?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
alok
Senior

If you are using the BLE-Mesh firmware, please use corresponding "ST BLE Mesh" App from play store

If you are using the Generic model for LED on-off: The entry point is "GenericModelServer_ProcessMessageCb()"

For Vendor Model, the implementation is in Vendor.c. The entry point for message from App is "Vendor_WriteLocalDataCb()". Similarly, the read message can be seen in "ReadLocalDataCb"