2023-08-03 10:06 PM
Here I'm using a USB Interface IC DRP for OTG. when I look into the datasheet for interfacing, I find some details in the pinout contrary to the diagram for pin numbers 16 and 17. Please someone clarify in this
Solved! Go to Solution.
2023-08-03 10:48 PM
Welcome @Aravind R, to the community!
Thank you very much for pointing this out! It is a typo in the numbering of the pin numbers of the TCPP03-M20 in the pin out drawing. If you look closely, you can see that
… 15 17 16 18 …
was numbered there by mistake.
Regards /Peter
2023-08-03 10:48 PM
Welcome @Aravind R, to the community!
Thank you very much for pointing this out! It is a typo in the numbering of the pin numbers of the TCPP03-M20 in the pin out drawing. If you look closely, you can see that
… 15 17 16 18 …
was numbered there by mistake.
Regards /Peter
2023-08-03 11:10 PM
Thanks peter