2023-09-13 7:17 AM
Hello, I measure the output differential voltage of the drivers (with 100ohm termination resistor) and it is always higher than 0.4V that is referred to the datasheet. What I measure is about 0.68V. Is that normal?
Thank you in advance
Solved! Go to Solution.
2023-09-13 7:30 AM - edited 2023-09-13 7:32 AM
Hello @DMala.1
Is this the test circuit you have used.
The datasheet values are according to this test circuit.
Best regards.
II
2023-09-13 7:30 AM - edited 2023-09-13 7:32 AM
Hello @DMala.1
Is this the test circuit you have used.
The datasheet values are according to this test circuit.
Best regards.
II
2023-09-13 7:30 AM
Related thread https://community.st.com/t5/interface-and-connectivity-ics/lvds-transceiver-rhflvdsr2d2-failure-info/td-p/590206
2023-09-13 8:48 AM
Was this chip supplied with 5V? In which case, all bets are off.
Unclear what the connection is between this thread and the other, or why you posted there.
2023-09-14 12:29 AM
Hello and thanks for the answers!
The chip is supplied with 3.3V and I measure on a termination resistor of 100Ohm as in picture 3 of the datasheet, what I don't use is the two capacitors.
2023-09-14 12:44 AM
To have a credible result, you should use the same conditions as described in the datasheet (you should use the 2 capacitors).
Best regards.
II