Skip to main content
Visitor II
September 13, 2023
Question

LVDS transceiver RHFLVDSR2D2 failure info

Good afternoon,

 

We are evaluating the possible consequence for the LVDS transceiver RHFLVDSR2D2 in case that it is supplied with a voltage above its absolute value which is 4,8V.

In particular we are asked to evaluate the case that voltage applied to supply is 5V: can you provide us some information to analyse this failure? Is possible to have an equivalent failure impedance to be considered from supply to inputs/output pins?

Also a very simple equivalent circuit of input/output would be very useful to analyse effects on interface in such failure case.

Kind regards

This topic has been closed for replies.

2 replies

Issamos
Super User
September 13, 2023

@FabioCamozzi76 

I don't think such evaluation exist. To do this I suggest you to test it yourself refering to the Test circuit in the datasheet of the components.

Best regards.

II

DMala.1
Associate II
September 13, 2023

Hello, I measure the output differential voltage of the drivers (with 100ohm termination resistor) and it is always higher than 0.4V that is referred to the datasheet. What I measure is about 0.68V. Is that normal? 

Thank you in advance