2015-01-09 09:46 AM
Hi,
I'm trying to customize the advertising packet, but it's unsuccessful so far.
I use STEVAL-IDB002V1
BlueNRG HW v3.0
BlueNRG FW v6.4
Motherboard FW v1.4
Since the command ACI_GAP_SET_DISCOVARABLE doesn't give much options I've tried to use HCI_LE_SET_ADVERTISING_PARAMETERS , HCI_LE_Set_Advertizing_Data, HCI_LE_SET_ADVERTISE_ENABLE.
The response to HCI_LE_SET_ADVERTISING_PARAMETERS and HCI_LE_SET_ADVERTISE_ENABLE is Unknown HCI Command.
Are these supported commands?
Is there any other way to customize the advertising and scan packet?
Thanks
2016-01-05 02:15 AM
Hi, I want use an X-NUCLEO-IDB05A1 on (STEVAL-IDB002V1) RF MOTHERBOARD (vers 3.0). How do you connect them?
Thanks2016-01-22 02:43 AM
Hi,
I need to use an X-NUCLEO-IDB05A1 on (STEVAL-IDB002V1) RF MOTHERBOARD (vers 3.0). Don't I may connect them with jumper cable male to female?Using X-NUCLEO-IDB05A1 can I sending broadcast messages without the use of the advertisment? I need to have a device that send broadcast messages and observer the messages of the other device.Thanks