2024-12-04 4:31 AM
Hi Team ,I was trying the BLE example application from GitHub in IAR Workbench. After a successful compile using IAR Workbench, the binary is not able to run on the eval board, and the board is not advertising the packet at all. However, when I run the existing binary available in the Binary folder, it works as expected. Could you please help me by providing the correct example code? i was using p2pserver_ota application .
2025-01-03 7:00 AM
Hello @reghund1985
After testing using the last STM32CubeWB V1.21.0, everything seems to be working fine. So, could you update to the last version of the stack (the one included on the CubeWB V1.21.0) and use the last version of the example for testing.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.