2022-09-29 04:54 AM
I have B-L462E-CELL1 development board with ST4SIM200M IC. this board came pre-provisioned with the Truphone profile but I didn't find any way to add a new profile. According to the datasheet eSIm chip supports up to 7 profiles but How can we add and switch between different profiles?
2025-01-21 12:35 AM
I also have same question i bouth st4sim-200 ic and want add more sim profiles. But dont know which tool to use for that action.
2025-01-21 03:40 AM
Hi, the ST4SIM-200 is configured with 1GLOBAL (former Truphone) connectivity, and 1GLOBAL is also configured as Subscription Management platform (SM-SR), able to manage remotely the profile on the eSIM.
According the GSMA SGP.02 specification/architecture, the new profile to be downloaded, shall be available on the SM-DP of the operator and the SM-DP integrated with the SM-SR managing the eSIM.
That said, the profile download shall be managed through SM-SR and in that case referring to 1GLOBAL.
The drawback/limitation of this architecture is that the SM-DP of the operator you want to download is not available on 1GLOBAL SM-SR.
2025-01-21 06:35 AM
Understand, but cannt add custom profile of my network provider. Or can it programing by some toolkit
2025-01-21 06:58 AM
It's not possible to program. The only way is through 1GLOBAL partner.
2025-01-21 07:06 AM - edited 2025-01-27 06:49 AM
@Agostino VANORE wrote:It's not possible to program. The only way is through 1GLOBAL partner.
Indeed.
@Kobra1991 @ffwali remember that the 'S' in "SIM" stands for "Subscriber" - ie, the one who pays for the service.
The SIM credentials are all about ensuring that the service provider gets paid - so they're not going to allow anyone to just go randomly creating SIMs!
#eSIM #SIMProfile
2025-01-30 02:26 AM
How can I program esim on chip with creditentials I receive from my provider, manually input?
Please recommend to me the esim on chip part and the device and programming tool?
2025-01-30 02:36 AM
You can't - as @Agostino VANORE explained.