2020-06-06 10:57 AM
I am using a BlueNRG-M2 as a Network Processor.
What is the method of programming these devices with the Network Processor code?
Can they be programmed with an ST_LINK?
2020-06-10 08:41 PM
Deleted
2020-06-11 08:55 PM
Sorry for mis-understanding the question previously.
Yes. ST-Link over SWD.
SWCLK: pin 12
SWDIO: pin 13
Two interfaces are supported: UART and SPI
Please program DTM pre-build image accordingly.