cancel
Showing results for 
Search instead for 
Did you mean: 

Getting started with X-Nucleo-IDW01M1, wifi connectevity + Nucleo-F446ZE

OLAAO.1
Associate

Hello,

I want to add the wifi module to my Nucleo-F446ZE board, and for that I'm using X-Nucleo-IDW01M1.

I know that the connection between the Nucleo BOARD and the WIFI module goes through UART. So, we must configure UART1 for the connection between the Nucleo board and the wifi module and then uart 2 for the connection with the PC. I looked for examples of TUTO, documentation, project carried out on other nucleo cards to get an idea on the configuration on STM32Cube and the AT commands used but I can't find anything. Is it possible to create a project and develop the wif module on STM32CUBEIDE with idw01M1? Should I use another module like ESP8266? Would someone have a track for this type of configuration, an example with another Nucleo board or anything that could help me with this problem?

Thinks :)

1 REPLY 1
Piranha
Chief II

UM1695