User Activity

Hello, I want to add the wifi module to my Nucleo-F446ZE board, and for that I'm using X-Nucleo-IDW01M1.I know that the connection between the Nucleo BOARD and the WIFI module goes through UART. So, we must configure UART1 for the connection between ...
Right at the moment I have 2 X-NUCELO WIFI expansion board, X-NUCLEO-IDW01M1 & X-NUCLEO-IDW04A1. I am pretty confused, which one to use for an NUCLEO-144 STM32-Cortex M4 ?Is there any difference between the 2 boards?Which one is easy to manipulate?t...