cancel
Showing results for 
Search instead for 
Did you mean: 

FCC Standards S2LP parameters for 902 – 928 MHz

Jutt
Associate II

Hi.

is there any example using  902 – 928 MHz just using S2LP(no Sigfox), which fulfill the FFC standards regarding to the frequency hopping. according to AN4949, my understanding , in SRadioInit base frequency would be 902 Mhz with frequency deviation will be 127Khz. is that correct or do i need to set more parameters.

0 REPLIES 0