2023-11-08 9:31 AM - edited 2023-11-08 9:38 AM
We are looking to add a pre qualified bluetooth module to a consumer product and the device live outdoors and periodically connect to a phone. We have identified the BlueNRG-1 as a candidate but perhaps there is a better choice. How well is the BlueNRG-1 supported and is it easy to get up and connected to a phone with sample code? Our requirements are:
-Pre certified (ideally CE marked)
-Price is a big factor, ideally $1-2 at high quantity (5000)
-Will be used to transmit data and over the air updates
-Low power sleep but good range required
-Industrial temp spec or better (-40 to 85C)
-Compatibility with microcontrollers from other vendors
-Newest protocols are better assuming they are backwards compatible
Other Questions:
-Are there emmulators for bluetooth such as the BlueNRG-1 to speed up software developement?
-Is there a ballpark range we can expect with the BlueNRG-1 (line of sight)?
-If we decided we needed WiFi and Bluetooth, are there cheap modules that can do both?